Labor Day Closure: We’ll be closed Monday, Sept. 7, and reopen Tuesday, Sept. 8.

Noise Figure to/from Noise Temperature Calculator

Noise figure to/from noise temperature calculator from Pasternack will produce either noise figure or noise temperature, depending on the input type.

When looking at noise figure (NF) calculator output, it measures degradation of the signal-to-noise ratio (SNR), caused by components, such as amplifiers, in an RF signal chain. The noise figure number, displayed in decibels (dB), represents the performance by which an amplifier or RF receiver can be measured.

For the noise temperature calculator, it is a representation of noise in terms of the temperature required to produce an equivalent amount of Johnson-Nyquist Noise. 

Calculation

 
 
 

Result:

Noise Figure:

Prefix Symbol Value
Tera 'T' 1012
Giga 'G' 109
Mega 'M' 106
kilo 'k' 103
Prefix Symbol Value
pico 'p' 10-12
nano 'n' 10-9
micro 'u' 10-6
milli 'm' 10-3